| Overload | Description |
|---|---|
| SetStates(CustomModulationConstellation,CustomModulationState[]) | Sets the modulation states that define this custom modulation. |
| SetStates(CustomModulationConstellation,Double[]) | Sets the modulation states that define this custom modulation. |
| SetStates(CustomModulationConstellation,Double[],Int64[]) | Sets the modulation states that define this custom modulation. |
| SetStates(CustomModulationConstellation,Double[],Int64[],Boolean) | Sets the modulation states that define this custom modulation. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)