Keysight 89600 VSA .NET API
EqualizationOptimizationMode Enumeration
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace : EqualizationOptimizationMode Enumeration


Glossary Item Box

Specifies the type of the optimizer used in the LMS equalizer.

Syntax

Visual Basic (Declaration) 
Public Enum EqualizationOptimizationMode 
   Inherits System.Enum
C# 
public enum EqualizationOptimizationMode : System.Enum 
C++/CLI 
public enum class EqualizationOptimizationMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
MinimizeErrorVectorThe second type of optimizer, which minimizes error vector, is enabled.
MinimizeEvmThe first type of optimizer, which minimizes EVM, is enabled.
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.20

See Also