| Visual Basic (Declaration) | |
|---|---|
Public Enum FrameDefinitionStyle Inherits System.Enum | |
| C# | |
|---|---|
public enum FrameDefinitionStyle : System.Enum | |
| C++/CLI | |
|---|---|
public enum class FrameDefinitionStyle : public System.Enum | |
| Member | Description | Minimum SW Version‡ |
|---|---|---|
| Burst | The frame does not repeat (burst of data followed by an idle period). The length of the frame is defined by FrameDefinition.Length. | — |
| Periodic | The frame repeats with a period defined by FrameDefinition.Length. | — |
| ‡ This is the minimum 89600 VSA software version level needed to use this enum member. | ||
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)