Keysight 89600 VSA .NET API
PhaseTrackingInterpolationMode Enumeration
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace : PhaseTrackingInterpolationMode Enumeration


Glossary Item Box

Determines the interpolation mode for phase tracking.

Syntax

Visual Basic (Declaration) 
Public Enum PhaseTrackingInterpolationMode 
   Inherits System.Enum
C# 
public enum PhaseTrackingInterpolationMode : System.Enum 
C++/CLI 
public enum class PhaseTrackingInterpolationMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AveragedThenNearestAveragedThenNearest: the phase offset is first averaged over the known segments, then the unknown segments are interpolated with the phase offset of the nearest known segments.
LinearInBetweenRepeatAtTwoEndsLinearInBetweenRepeatAtTwoEnds: the phase offsets of the unknown segments is linear interpolated if they are in between the known segments, and repeat with the nearest phase offset if they are at the two ends.
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also