Keysight 89600 VSA .NET API
ReferenceFrequencyDefinition Enumeration
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace : ReferenceFrequencyDefinition Enumeration


Glossary Item Box

Reference Frequency Definition.

Syntax

Visual Basic (Declaration) 
Public Enum ReferenceFrequencyDefinition 
   Inherits System.Enum
C# 
public enum ReferenceFrequencyDefinition : System.Enum 
C++/CLI 
public enum class ReferenceFrequencyDefinition : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AssignedMeasurementChannelCenterThe reference frequency of a component carrier is defined to be the center of the measurement channel assigned to the component carrier.
ManuallySpecifiedThe reference frequency of a component carrier is manually specified.
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.40

See Also