Keysight 89600 VSA .NET API
SequenceResetSymbolIndex Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > Scrambler Class : SequenceResetSymbolIndex Property


Glossary Item Box

Gets or sets the symbol location where the scrambling sequence is reset. This is an offset from the beginning of the frame.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SequenceResetSymbolIndex As Integer
C# 
public abstract int SequenceResetSymbolIndex {get; set;}
C++/CLI 
public:
abstract property int SequenceResetSymbolIndex {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also