Keysight 89600 VSA .NET API
SequenceType Enumeration
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace : SequenceType Enumeration


Glossary Item Box

Specifies the type of scrambling to perform.

Syntax

Visual Basic (Declaration) 
Public Enum SequenceType 
   Inherits System.Enum
C# 
public enum SequenceType : System.Enum 
C++/CLI 
public enum class SequenceType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
DvbS2S2xPlframeDVB-S2/S2X PLFRAME scrambling as described in section 5.5.4 of EN 302 307-1.
DvbS2xSuperFrameDVB-S2X Super-Frame scrambling as described in section E.2.4 of EN 302 307-2.
Ieee80211Aday802.11ad/ay scrambling.
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00

See Also