Keysight 89600 VSA .NET API
PatternSearchSymbolOffset Property
See Also 
Keysight.SA.Vsa.FlexFrame.Interfaces Assembly > Keysight.SA.Vsa.FlexFrame Namespace > SingleCarrier Class : PatternSearchSymbolOffset Property


Glossary Item Box

Gets or sets the offset in symbols from the start of the frame to the beginning symbol of the search pattern.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PatternSearchSymbolOffset As Integer
C# 
public abstract int PatternSearchSymbolOffset {get; set;}
C++/CLI 
public:
abstract property int PatternSearchSymbolOffset {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also