Equalizer Training (802.16 OFDM)
: See 802.16 OFDM Standard Setups/Presets Table.
When demodulating the 802.16 OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. signal, the VSA uses an equalizer to correct for linear impairments in the signal path, such as multi-path. The 89600 VSA supports two different methods to initialize, or "train," the equalizer: and . Switching between the two methods can help isolate problems contributing to increased RCE Relative Constellation Error is the RMS level of the Error Vector Magnitude, averaged over all subcarriers and all detected OFDM symbols. (EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format.).
Preamble Only
The equalizer is trained by looking at the Channel Estimation Sequence in the preamble of the OFDM burst. After this initialization, the equalizer coefficients are held constant while demodulating the rest of the burst.

Advantages of this method of equalization include the following:
- It models what a typical OFDM receiver would do, so the RCE (EVM) measured using this method more accurately reflects the signal quality seen by a typical OFDM receiver.
- It complies with the description in the "Transmit constellation error and test method" section (8.3.10.1.2) of the 802.16a/d standard.
The disadvantage of this method is that the measured RCE (EVM) value may be higher for signals whose impairments change during the burst than it would be if the equalizer were trained over the entire burst.
The default value is Preamble Only.
Preamble & Data
The equalizer is trained by analyzing the entire OFDM burst, including the Channel Estimation Sequence (contained in the preamble) and the Data symbols. This type of training generally gives a more accurate estimate of the true response of the transmission channel.
Advantages of this method of equalization include the following:
- The equalizer coefficients typically reflect the linear channel impairment with greater accuracy, as the data set used to train the equalizer is larger and is less affected by turn-on transient effects in the burst.
- The RCE (EVM) is typically lower because the equalizer is less impacted by noise and some other forms of distortion. (RCE (EVM) represents the error due to noise, non-linear distortion, spurious, and residual linear distortion.)
The disadvantage of this method is that it is less likely to accurately reflect the performance of a typical OFDM receiver. Because this type of equalizer computation is more complicated and therefore more expensive to implement, it is less likely to be used in practical receivers.
Further Information
For details about equalization, see application note 1455 "Keysight Equalization Techniques and OFDMA Troubleshooting for Wireless LANs" in the Keysight 89600 VSA Product & Application Notes help.
See Also