Advanced Tab (802.16 OFDM)
The tab of the dialog box configures advanced parameters used to demodulate user defined and/or nonstandard 802.16 OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. signals and to manipulate trace data results.
The tab dialog box configures these parameters:
- Equalizer
Training
- Preamble Only
- Preamble & Data
- Mirror Frequency Spectrum
- Normalize IQ Traces
- Pilot Tracking
- Subcarrier
Selection
- All
- Single Subcarrier
- Pilots Only
- Subchannel Index
- Symbol Time Adjustment
See Also
IEEE 802.16 OFDM Demod Properties Dialog Box