Automatic - Result Length (802.16 OFDM)
: See 802.16 OFDM Standard Setups/Presets Table.
When (Default) in Result Length is selected, the VSA automatically determines the measurement result length. The Result Length is determined by comparing the input signals symbol-time length to the Max Result Length and using the smaller value
See Result Length Parameters for more information about how the VSA determines the measurement result length in , and modes.
The following figures illustrate how the VSA determines the measurement result length in mode when the is greater than (Fig. 1) and less than (Fig. 2) the symbol-times detected within the burst.
The measurement result length will default to the number of symbol-times detected within the burst.

The measurement result length is set to the .

See Also
Result Length Parameters (802.16 OFDM)