CDF (802.16 OFDM Demodulation)
trace data displays the cumulative distribution function (CDF Cumulative Distribution Function: The cumulative probability that a parameter will be less than a given value X.) for the selected input channel. is computed by integrating the PDF (Probability Density Function).
The is computed from the segment of the OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. burst specified by the and . If the Offset is zero and the Interval is equal to the result length, the burst preamble is included in the CDF.
For more information, see CCDF.
See Also