Available Trace Data (802.16 OFDM)
The following table provides a list of the available measurement trace data for 802.16 OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. modulation analysis. Click on the name for detailed information about each Trace Data result.
| 
                             OFDM Demodulation   | 
                    |
|---|---|
See Also