Active Zone (802.16 OFDMA)
: (See OFDMA Standard Presets Table.)
selects the zone from the defined map to use for analysis. The selected zone also becomes the active zone for editing on the tab.
See Also
: (See OFDMA Standard Presets Table.)
selects the zone from the defined map to use for analysis. The selected zone also becomes the active zone for editing on the tab.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |