Using a Standard Preset (802.16 OFDMA)
configures the VSA to demodulate and measure a particular OFDMA signal that conforms to a profile of the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.16e OFDMA standard specification. will configure the , , and parameters to match the specified profile. All other OFDMA parameters will be reset to a default state as described in the following "Preset to Standard Default" tables.
also defaults to Definition Source mode and a default zone definition, the current manual analysis zone and data burst definitions will be lost.
To configure the VSA. click the control and select one of the listed OFDMA preset configurations.
1) The 802.16 OFDMA Demodulator must be selected before these Standard Presets are available.
2) For a description of the profiles, see the Standard parameter topic.
|
Preset
to Standard |
Description |
|---|---|
|
8.75 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. profile defined in IEEE 802.16e OFDMA standard. |
|
|
5 MHz profile defined in IEEE 802.16e OFDMA standard |
|
|
10 MHz profile defined in IEEE 802.16e OFDMA standard |
|
Property Tab |
Parameter |
Downlink |
Uplink |
|---|---|---|---|
|
IEEE 802.16 OFDMA |
IEEE 802.16 OFDMA |
||
|
|
Nominal BW |
5 MHz |
5 MHz |
|
|
512 |
512 |
|
|
|
Bandwidth Ratio |
28/25 |
28/25 |
|
|
Guard Interval |
1/8 |
1/8 |
|
|
Frame Length |
5 ms |
5 ms |
|
|
Downlink Frame Ratio |
.5 |
.5 |
|
|
Preamble Index |
0 |
na |
|
|
Override Preamble Definition |
cleared |
na |
|
|
IDCell |
0 |
na |
|
|
Segment |
0 |
na |
|
|
Subchannel Group Bitmask |
63 |
na |
|
|
Enable Burst Analysis |
selected |
selected |
|
|
Enable Defined Burst Boosting Levels |
selected |
na |
| Definition Source | Manual | Manual | |
|
|
Zone Definition |
DL Down Link (forward link: from base station to cell phone)-PUSC partial usage of subchannels: Some of the subchannels are allocated to the transmitter. |
UL Up Link (reverse link: from cell phone to base station)-PUSC |
|
|
Use all Subchannels |
cleared |
na |
| Dedicated Pilots | cleared | na | |
| No STC/MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. | na | ||
| STC Matrix | A | na | |
|
|
PrbsID |
1 |
na |
| Override IDCell with PermBase | selected and 0 | na | |
|
|
Offset |
1 Symbols |
0 Symbols |
|
|
Length |
20 Symbols |
12 Symbols |
| Use Subchannel Rotation | na | selected | |
|
|
PermBase |
na |
1 |
| Definition Type (defining bursts) | FCH | CDMA Code Division Multiple Access: One of several digital wireless transmission methods in which signals are encoded using a specific pseudo-random sequence, or code, to define a communication channel. A receiver, knowing the code, can use it to decode the received signal in the presence of other signals in the channel. This is one of several "spread spectrum" techniques, which allows multiple users to share the same radio frequency spectrum by assigning each active user an unique code. CDMA offers improved spectral efficiency over analog transmission in that it allows for greater frequency reuse. Other characteristics of CDMA systems reduce dropped calls, increase battery life and offer more secure transmission. See also IS-95. and FFB | |
| Allocation Geometry | Rectangular | Rectangular | |
| Data Tone Modulation | QPSK Quadrature phase shift keying
|
16-QAM Quadrature Amplitude Modulation | |
| Boosting Level | 0 dB | na | |
| STC Mode | na | None | |
| Pilot Pattern | na | A | |
| Measure Input Channel | Channel 1 | Channel 1 | |
| Enable Matrix Decoder | cleared | cleared | |
| Measure Matrix Stream | Stream 1 | Stream 1 | |
| Override Transmit Antenna Pilot Pattern | cleared and Sync to Transmit Anntenna 0 | cleared and Sync to Transmit Antenna 0 | |
| Enable Cyclic Delay Diversity (CDD Cyclic Delay Diversity (CDD): To avoid unintentional beamforming, the IEEE 802.11n draft standard uses a process known as Cyclic Delay Diversity (CDD), which basically offsets each spatial stream by a different constant, non-coherent delay. The offset considerably lowers the likelihood of correlated signals being transmitted by two or more antennas. This, in conjunction with a pseudorandom scrambler run over the transmitted data bits, ensures that the likelihood of two spatial streams correlating is very low.) Measurement | cleared | cleared | |
| Include inactive Antenna Path on MIMO Traces | cleared | cleared | |
| Normalize each MIMO Path in Frequency Response | selected | selected | |
|
|
Acquistion Length |
1 Frames |
1 Frames |
|
|
Analysis Offset |
0 Frames |
0 Frames |
|
|
Pulse Search |
selected |
selected |
|
|
Sync Search Offset |
na |
cleared and 0 Symbols |
| Include Zone Offset | na | cleared | |
|
|
Override Measurement Region (demodulation) |
cleared |
cleared |
|
Measurement Offset |
0 Symbols | 0 Symbols | |
| Measurement Interval | 1 Symbols | 1 Symbols | |
| Measurement Region (non-demod) | Demodulation | Demodulation | |
| Include Transition Regions | cleared | cleared | |
|
|
Enable additional demodulator settings | cleared | cleared |
| Restrict bandwidth to standard values | selected | selected | |
| Compensation | Compensate IQ Mismatch | cleared | cleared |
|
|
Mirror Frequency Spectrum |
cleared |
cleared |
|
|
Enable Multicarrier Filter |
selected |
selected |
|
|
Symbol Time Adjustment |
-3.125% |
-3.125% |
| Display Options | Burst Power is Per-subcarrier | selected | selected |
|
|
Compensate Modulation PRBS Pseudo-Random Binary Sequence (de-rotate) |
cleared |
cleared |
|
Normalize IQ Traces |
selected |
selected |
|
|
Decoding |
cleared |
na |
|
|
|
UL-MAP Decoding |
selected |
na |
| Decode to Map | selected | na | |
|
|
Disable Data Tone Modulation Autodetect (use burst definitions) |
cleared |
cleared |
|
Equalizer Training |
Preamble Only |
cleared |
na |
| Preamble, pilots and data |
selected |
na |
|
| Preamble and pilots |
cleared |
na |
|
| No equalization |
na |
cleared |
|
| Pilots and data |
na |
selected |
|
| Pilots Only |
na |
cleared |
|
| Enable Equalizer Smoothing Filter | cleared |
cleared |
|
|
Pilot Training |
Track Amplitude |
clear |
selected |
| Track Phase |
selected |
selected |
|
| Track Timing |
selected |
selected |
|
|
Subcarrier Subset Selection |
Select Subcarrier Region |
cleared |
cleared |
| Subcarrier Offset | 1 | 1 | |
| Subcarrier Interval | 1 | 1 | |
|
Standard Interpretation |
Use Cor1/D2 DL-PUSC cluster renumbering |
na |
na |
|
Notes: |
|||
|
Property Tab |
Parameter |
Downlink |
Uplink |
|---|---|---|---|
|
IEEE 802.16 OFDMA |
IEEE 802.16 OFDMA |
||
|
|
Nominal BW |
10 MHz |
10 MHz |
|
|
FFT Length |
1024 |
1024 |
|
|
Bandwidth Ratio |
28/25 |
28/25 |
|
|
Guard Interval |
1/8 |
1/8 |
|
|
Frame Length |
5 ms |
5 ms |
|
|
Downlink Frame Ratio |
.5 |
.5 |
|
|
Preamble Index |
0 |
na |
|
|
Override Preamble Definition |
cleared |
na |
|
|
IDCell |
0 |
na |
|
|
Segment |
0 |
na |
|
|
Subchannel Group Bitmask |
63 |
na |
|
|
Enable Burst Analysis |
selected |
selected |
|
|
Enable Defined Burst Boosting Levels |
selected |
na |
| Definition Source | Manual | Manual | |
|
|
Zone Definition |
DL-PUSC |
UL-PUSC |
|
|
Use all Subchannels |
cleared |
na |
| Dedicated Pilots | cleared | na | |
|
STC Mode |
No STC/MIMO | na | |
| STC Matrix | A | na | |
|
|
PrbsID |
1 |
na |
| Override IDCell with PermBase | selected and 0 | na | |
|
|
Offset |
1 Symbols |
0 Symbols |
|
|
Length |
20 Symbols |
15 Symbols |
| Use Subchannel Rotation | na | selected | |
|
|
PermBase |
na |
1 |
| Definition Type (defining bursts) | FCH | CDMA and FFB | |
| Allocation Geometry | Rectangular | Rectangular | |
| Data Tone Modulation | QPSK |
16-QAM | |
| Boosting Level | 0 dB | na | |
| STC Mode | na | None | |
| Pilot Pattern | na | A | |
| Measure Input Channel | Channel 1 | Channel 1 | |
| Enable Matrix Decoder | cleared | cleared | |
| Measure Matrix Stream | Stream 1 | Stream 1 | |
| Override Transmit Antenna Pilot Pattern | cleared and Sync to Transmit Anntenna 0 | cleared and Sync to Transmit Antenna 0 | |
| Enable Cyclic Delay Diversity (CDD) Measurement | cleared | cleared | |
| Include inactive Antenna Path on MIMO Traces | cleared | cleared | |
| Normalize each MIMO Path in Frequency Response | selected | selected | |
|
|
Acquistion Length |
1 Frames |
1 Frames |
|
|
Analysis Offset |
0 Frames |
0 Frames |
|
|
Pulse Search |
selected |
selected |
|
|
Sync Search Offset |
na |
cleared and 0 Symbols |
| Include Zone Offset | na | cleared | |
|
|
Override Measurement Region (demodulation) |
cleared |
cleared |
|
Measurement Offset |
0 Symbols | 0 Symbols | |
| Measurement Interval | 1 Symbols | 1 Symbols | |
| Measurement Region (non-demod) | Demodulation | Demodulation | |
| Include Transition Regions | cleared | cleared | |
|
|
Enable additional demodulator settings | cleared | cleared |
| Restrict bandwidth to standard values | selected | selected | |
| Compensation | Compensate IQ Mismatch | cleared | cleared |
|
|
Mirror Frequency Spectrum |
cleared |
cleared |
|
|
Enable Multicarrier Filter |
selected |
selected |
|
|
Symbol Time Adjustment |
-3.125% |
-3.125% |
| Display Options | Burst Power is Per-subcarrier | selected | selected |
|
|
Compensate Modulation PRBS (de-rotate) |
cleared |
cleared |
|
Normalize IQ Traces |
selected |
selected |
|
|
Decoding |
DL-MAP Decoding |
cleared |
na |
|
|
UL-MAP Decoding |
selected |
na |
| Decode to Map | selected | na | |
|
|
Disable Data Tone Modulation Autodetect (use burst definitions) |
cleared |
cleared |
|
Equalizer Training |
Preamble Only |
cleared |
na |
| Preamble, pilots and data |
selected |
na |
|
| Preamble and pilots |
cleared |
na |
|
| No equalization |
na |
cleared |
|
| Pilots and data |
na |
selected |
|
| Pilots Only |
na |
cleared |
|
| Enable Equalizer Smoothing Filter | cleared |
cleared |
|
|
Pilot Training |
Track Amplitude |
clear |
selected |
| Track Phase |
selected |
selected |
|
| Track Timing |
selected |
selected |
|
|
Subcarrier Subset Selection |
Select Subcarrier Region |
cleared |
cleared |
| Subcarrier Offset | 1 | 1 | |
| Subcarrier Interval | 1 | 1 | |
|
Standard Interpretation |
Use Cor1/D2 DL-PUSC cluster renumbering |
na |
na |
|
Notes: |
|||
|
Preset to Standard: TTA Telecommunications Technology Association (Korea): A telecommunications standards setting body in Korea.-Phase2 (WiBro |
|||
|---|---|---|---|
|
Property Tab |
Parameter |
Downlink |
Uplink |
|
IEEE 802.16 OFDMA |
IEEE 802.16 OFDMA |
||
|
|
Nominal BW |
8.75 MHz |
8.75 MHz |
|
|
FFT Length |
1024 |
1024 |
|
|
Bandwidth Ratio |
8/7 |
8/7 |
|
|
Guard Interval |
1/8 |
1/8 |
|
|
Frame Length |
5 ms |
5 ms |
|
|
Downlink Frame Ratio |
.63952 |
.63952 |
|
|
Preamble Index |
0 |
na |
|
|
Override Preamble Definition |
cleared |
na |
|
|
IDCell |
0 |
na |
|
|
Segment |
0 |
na |
|
|
Subchannel Group Bitmask |
63 |
na |
|
|
Enable Burst Analysis |
selected |
selected |
|
|
Enable Defined Burst Boosting Levels |
selected |
na |
| Definition Source | Manual | Manual | |
|
|
Zone Definition |
DL-PUSC |
UL-PUSC |
|
|
Use all Subchannels |
cleared |
na |
| Dedicated Pilots | cleared | na | |
|
STC Mode |
No STC/MIMO | na | |
| STC Matrix | A | na | |
|
|
PrbsID |
1 |
na |
| Override IDCell with PermBase | selected and 0 | na | |
|
|
Offset |
1 Symbols |
0 Symbols |
|
|
Length |
20 Symbols |
15 Symbols |
| Use Subchannel Rotation | na | selected | |
|
|
PermBase |
na |
1 |
| Definition Type (defining bursts) | FCH | CDMA and FFB | |
| Allocation Geometry | Rectangular | Wrapped | |
| Data Tone Modulation | QPSK |
16-QAM | |
| Boosting Level | 0 dB | na | |
| STC Mode | na | None | |
| Pilot Pattern | na | A | |
| Measure Input Channel | Channel 1 | Channel 1 | |
| Enable Matrix Decoder | cleared | cleared | |
| Measure Matrix Stream | Stream 1 | Stream 1 | |
| Override Transmit Antenna Pilot Pattern | cleared and Sync to Transmit Anntenna 0 | cleared and Sync to Transmit Antenna 0 | |
| Enable Cyclic Delay Diversity (CDD) Measurement | cleared | cleared | |
| Include inactive Antenna Path on MIMO Traces | cleared | cleared | |
| Normalize each MIMO Path in Frequency Response | selected | selected | |
|
|
Acquistion Length |
1 Frames |
1 Frames |
|
|
Analysis Offset |
0 Frames |
0 Frames |
|
|
Pulse Search |
selected |
selected |
|
|
Sync Search Offset |
na |
cleared and 0 Symbols |
| Include Zone Offset | na | cleared | |
|
|
Override Measurement Region (demodulation) |
cleared |
cleared |
|
Measurement Offset |
0 Symbols | 0 Symbols | |
| Measurement Interval | 1 Symbols | 1 Symbols | |
| Measurement Region (non-demod) | Demodulation | Demodulation | |
| Include Transition Regions | cleared | cleared | |
|
|
Enable additional demodulator settings | cleared | cleared |
| Restrict bandwidth to standard values | selected | selected | |
| Compensation | Compensate IQ Mismatch | cleared | cleared |
|
|
Mirror Frequency Spectrum |
cleared |
cleared |
|
|
Enable Multicarrier Filter |
selected |
selected |
|
|
Symbol Time Adjustment |
-3.125% |
-3.125% |
| Display Options | Burst Power is Per-subcarrier | selected | selected |
|
|
Compensate Modulation PRBS (de-rotate) |
cleared |
cleared |
|
Normalize IQ Traces |
selected |
selected |
|
|
Decoding |
DL-MAP Decoding |
cleared |
na |
|
|
UL-MAP Decoding |
selected |
na |
| Decode to Map | selected | na | |
|
|
Disable Data Tone Modulation Autodetect (use burst definitions) |
cleared |
cleared |
|
Equalizer Training |
Preamble Only |
cleared |
na |
| Preamble, pilots and data |
selected |
na |
|
| Preamble and pilots |
cleared |
na |
|
| No equalization |
na |
cleared |
|
| Pilots and data |
na |
selected |
|
| Pilots Only |
na |
cleared |
|
| Enable Equalizer Smoothing Filter | cleared |
cleared |
|
|
Pilot Training |
Track Amplitude |
clear |
selected |
| Track Phase |
selected |
selected |
|
| Track Timing |
selected |
selected |
|
|
Subcarrier Subset Selection |
Select Subcarrier Region |
cleared |
cleared |
| Subcarrier Offset | 1 | 1 | |
| Subcarrier Interval | 1 | 1 | |
|
Standard Interpretation |
Use Cor1/D2 DL-PUSC cluster renumbering |
na |
na |
|
Notes: |
|||
See Also