Use all Subchannels (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
(applies to only)
determines how the subchannels are allocated for the DL Down Link (forward link: from base station to cell phone)-PUSC partial usage of subchannels: Some of the subchannels are allocated to the transmitter. zone analysis.
-
: Non-segmented DL-PUSC analysis is enforced, the parameter is ignored and all subchannels are assumed to be allocated to the zone.
-
: Segmented DL-PUSC analysis is allowed and and are used to determine which subchannels are allocated to the analyzed segment.
This parameter only applies to Zone Definition in the Z tab.
See Also