Use Subchannel Rotation (802.16 OFDMA)
: Selected (See OFDMA Standard Presets Table.)
(applies to only)
The check box determines if the logical subchannel rotation algorithm is applied to the zone permutation algorithm.
: Subchannel rotation algorithm is applied to the zone permutation algorithm.
; Subchannel rotation algorithm is not applied to the zone permutation algorithm.
See the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.16e-2005 standard for more details about the UL Up Link (reverse link: from cell phone to base station)-PUSC partial usage of subchannels: Some of the subchannels are allocated to the transmitter. permutation algorithm.
See Also