Preamble Frequency Error (802.16 OFDMA)
(applies to Only)
is the difference between the measured center frequency of the transmitted signal and the 89600 center frequency. The trace shows the total frequency error during the preamble portion of the OFDMA burst. This includes the constant frequency error displayed in the Syms/Errs trace data, in addition to any time-varying frequency error.
is sampled at BW*BWRatio..
See Also