RE Power Heatmap (5G NR/5G-Advanced)

There are two types of traces in the Trace > Data > Demod and MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. menus that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Display parameter). See About Per-Carrier Trace Types for more information.

RE Power Heatmap displays a two-dimensional representation of Resource Element (RE) Power for the reference component carrier with measurement symbols on the X axis, carriers on the Y axis, and Power (in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) represented by color (similar to Spectrogram). See the RE Power 3D trace for a three-dimensional view of RE Power data.

See Also

RE Power 3D Trace

Detected Allocations Time Trace

Available Trace Data