Resolution and Video Bandwidth

Power Spectrum measurements let you set both the Resolution Bandwidth (RBW Resolution Band Width (RBW or ResBW): specifies the minimum frequency bandwith that two separate frequency spectra can be resolved and viewed seperately. For FFT (digital) based VSA's the process is equivalent to passing a time-domain signal through a bank of bandpass filters, whose center frequencies correspond to the frequencies of the FFT bins. For a traditional swept-tuned (non-digital) spectrum analyzer, the resolution bandwidth is the bandwidth of the IF filter which determines the selectivity.) and the Video Bandwidth (VBW). You can manually set these parameters, or you can set the Span-to-ResBW ratio and/or VBW-to-ResBW ratio to automatically set these values. You can also set the maximum FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. size.

Resolution Bandwidth

The standard swept analyzer uses the last in a series of analog IF filters to determine resolution bandwidth.

In contrast, the 89600 VSA software with PXI hardware uses a digital IF and a DSP algorithm to determine resolution bandwidth (RBW). The minimum and maximum RBW for Power Spectrum measurements is determined by these parameters:

The narrowest practical RBW with Power Spectrum measurements is constrained by the length of time you are willing to wait for a measurement to be performed. The widest RBW is limited by the frequency span. The maximum RBW decreases as you narrow the frequency span and increases as you increase the frequency span.

ResBW Parameters

The ResBW Tab (Analysis > ResBW) lets you set the following parameters:

 

Max FFT Size

The Max FFT Size parameter lets you set the maximum FFT size to allow for power spectrum measurements. Larger sizes can use significantly more computer memory but can result in faster sweeps, especially at high Span to RBW ratios. This parameter is ignored for zero span measurements.