Inst Spectrum (Negative Peak) (Spectral Emissions Mask)
Inst Spectrum (Negative Peak) displays the instantaneous output from the Negative Peak detector. When measurement averaging is disabled, the Spectrum (Negative Peak) and Inst Spectrum (Negative Peak) displays are identical.
See the SEM Spectrum Trace Data Block Diagram and Detectors and Power Spectrum Analysis for more information.
The Inst Spectrum (Negative Peak) trace is only available when the Negative Peak detector is enabled.
Inst Spectrum (Negative Peak) may be channelized when multiband spectrum is in use, providing trace results for each spectrum/measurement channel shown on the Frequency tab.
See Also