Inst Spectrum (Sample) (Spectral Emissions Mask)
Inst Spectrum (Sample) displays the instantaneous output from the Sample detector. When measurement averaging is disabled, the Spectrum (Sample) and Inst Spectrum (Sample) displays are identical.
See the SEM Spectrum Trace Data Block Diagram and Detectors and Power Spectrum Analysis for more information.
The Inst Spectrum (Sample) trace is only available when the Sample detector is enabled.
Inst Spectrum (Sample) may be channelized when multiband spectrum is in use, providing trace results for each spectrum/measurement channel shown on the Frequency tab.
See Also