Acquisition Length (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Capture

When Segmented Capture mode is disabled, Acquisition Length specifies the total measurement acquisition length in seconds over which the detection and calculation will be performed. Any valid pulses detected will be reported within the pulse analysis results.

When Segmented Capture mode is enabled, the Acquisition Length parameter is grayed-out (unavailable) since user should specify desired Segmented Capture mode acquisition length using the Segment Length property.