Max Detection Count (Advanced-Radar/Hopping)

Analysis > Advanced-Radar/Hopping Measurement Properties > Detection Tab > Region Panel

When the Max Detection Count checkbox is enabled, you can specify an upper limit to the number of detected signal pulses which should be considered for inclusion within pulse analysis results. If the measured signal contains more valid pulses than the specified Max Detection Count, only the first Max Detection Count number of detected signal pulses will be processed and reported within the pulse analysis results.

When the Max Detection Count checkbox is disabled, all valid detected signal pulses within the Acquisition Length time interval will be reported within the pulse analysis results.

If you are unable to set your desired max detection count, make sure the Max Detection Count checkbox is checked (enabled).