Amplitude Ref Time (Advanced-Radar/Hopping)
Menu Path:
This trace is only available when the Synchronization Domain is Amplitude or the Pulsed checkbox is checked. If both of these are not true, the trace won't be available for selection.
Amplitude Ref Time reports region-synchronized reference signal amplitude level samples over time in the units determined by Trace Y Scale and Trace Format selection combination. The reference signal is the VSA's best guess as to what the intended pulse should have been.
Valid trace Format selections are:
- Real
The Ripple Analysis Width is displayed as a dark green band that is centered on each pulse.