Synchronization Domain (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > <all tabs>

Synchronization Domain specifies the domain of interest in which detection will take place. Synchronization Domain is provided on every tab because it is a fundamental configuration parameter affecting the entire Advanced-Radar/Hopping measurement. Synchronization domain-specific detection settings are located on the Detection tab > Region panel.

See Also

Advanced-Radar/Hopping Measurement Properties Dialog Box

Capture Tab

Detection Tab

Analysis Tab

Calculation Tab