Payload Pattern (Bluetooth)

Default: Auto

Payload Pattern selects the test payload the demodulator expects in the analyzed burst. The RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz).-PHY Physical Layer Test Specification defines different payloads for different transmitter tests, so the pattern determines which modulation-characteristics results are meaningful for a given capture:

See Also

Demod Tab

PDU Whitening

Results Table