Demod Tab (Bluetooth)

The Demod tab of the Bluetooth Demod Properties dialog box configures how the demodulator interprets the payload of the selected burst and which portion of the burst is used for the output power result.

The signal-description settings in the Bluetooth Mode Configuration section above the tabs (PHY Family, PHY Rate, Packet Type, and Channel Index) are shared by both Bluetooth measurements and are described in Common Properties.

The tab contains these parameters:

See Also

Bluetooth Demod Properties Dialog Box

Time Tab

Common Properties (Bluetooth)