Access Address (Bluetooth)
0x8E89BED6
Access Address sets the 32-bit access address (in hexadecimal) that the demodulator correlates against to locate the burst. This parameter is shown only when Burst Search Mode is set to .
For packet types whose access address is fixed by the standard, the entered value is ignored and the standard value is used. The effective access address is:
|
Packet Type |
Effective access address |
|
LE Advertising |
0x8E89BED6 (fixed by the standard) |
|
LE Test |
0x71764129 (fixed by the standard for direct test mode) |
|
LE Data |
The entered value |
|
Auto |
Determined for each burst: the entered value is tried as a candidate alongside the two standard-fixed addresses above, and the address that correlates best identifies the burst. The entered value is what this parameter reads back. |
See Also