Time Tab (Bluetooth)

The Time tab of the Bluetooth Demod Properties dialog box configures how the demodulator searches for Bluetooth bursts in the acquired time record and which detected burst is analyzed.

The signal-description settings in the Bluetooth Mode Configuration section above the tabs (PHY Family, PHY Rate, Packet Type, and Channel Index) are shared by both Bluetooth measurements and are described in Common Properties.

The tab contains these parameters:

The bursts found within the search length are listed in the Burst Table trace.

See Also

Bluetooth Demod Properties Dialog Box

Demod Tab

Common Properties (Bluetooth)