Burst Threshold (Bluetooth)
10 dB
Burst Threshold sets the level, in dB above the estimated noise floor, that the signal envelope must exceed to be detected as a burst.
This parameter is shown only when Burst Search Mode is set to . Lower the threshold to detect weak bursts; raise it if noise or adjacent signals are falsely detected as bursts.
See Also