Demod Bits (Bluetooth)
The trace shows the demodulated bit stream of the analyzed burst. If PDU Whitening applies, the bits are shown after de-whitening.
Use this trace to verify the transmitted payload — for example, to confirm that the device under test is sending the expected Payload Pattern for the modulation-characteristics tests.
A summary block above the bit stream identifies the packet the bits came from:
-
Burst — the number of the analyzed burst, matching its row in the Burst Table.
-
Packet Type — the configured , or the detected one when it is set to .
-
Coding — the active PHY Physical Layer rate.
-
Payload Length — the decoded payload length, in bits. Absent when the packet header did not decode.
-
Payload — the payload pattern the analyzer measured, such as or .
-
CRC Cyclic Redundancy Check — , , or when the CRC was not checked.
-
Sync — whether the burst synchronized.
When the selected burst never synchronized, this trace and the Demod Waveform trace show a indicator, and the bits shown are not meaningful. Check the column of the Burst Table to find a burst that did synchronize.
See Also