Inst Spectrum (Bluetooth)

The Inst Spectrum (Instantaneous Spectrum) trace is the frequency spectrum of the pre-demodulated time data. The time data is windowed and passed through an FFT to create the Inst Spectrum display.

If averaging is on, the Inst Spectrum does not show the effects of averaging. To see the effects of averaging, use the Spectrum trace data.

See Also

Time Trace

Spectrum Trace