Bluetooth Spectrum Properties Dialog Box
The dialog box contains the parameters that configure the spectrum-domain Bluetooth transmitter tests.
The Bluetooth Spectrum measurement type must be selected before this dialog box is available. To enable the measurement, click .
The section at the top of the dialog box holds the settings that are shared by both Bluetooth measurements (PHY Physical Layer family and rate, packet type, and channel index). See Common Properties for details.
Below it, the dialog box contains one tab:
-
Setup Tab — test purpose, channel power calculation, detector, and the specification limits.
See Also