Spectrum (Peak) (Bluetooth Spectrum)

Spectrum (Peak) is the output of the Peak detector after measurement averaging. When measurement averaging is enabled, it is the average of Inst Spectrum (Peak) over the number of traces set by Count, and the averaging style and count (for example, "RMS:10") are shown at the top of the trace display. When measurement averaging is off, the two traces are identical.

This is acquisition trace data and is shown for every enabled detector. It is not the Bluetooth Spectrum measurement result: the analyzed spectrum, with its Spec Limit line, is the Spectrum trace under the Bluetooth Spectrum group.

See Detectors and Power Spectrum Analysis for how each detector reduces the measured bins.

This trace is available only while the Peak detector is enabled on the Detectors tab. Bluetooth Spectrum enables the detector selected by Detector automatically; any other detector must be enabled by hand.

See Also

Inst Spectrum (Peak)

Spectrum (Bluetooth Spectrum)

Available Trace Data