Noise Correction Spectrum (Bluetooth Spectrum)
is the measured noise reference that is subtracted from the acquired spectrum while Noise Correction is on. Noise correction may affect measurement speed; see Noise Correction for more information.
Selecting a Test Purpose sets Noise Correction to the value that test is specified with, and re-applies it whenever the purpose is applied. turns Noise Correction off.
This trace is available only while the measurement’s active input domain is . See Preferred Input Domains.
See Also