Inst Spectrum (Average) (Bluetooth Spectrum)

Inst Spectrum (Average) is the instantaneous output of the Average detector, before measurement averaging is applied. When measurement averaging is off, Inst Spectrum (Average) and Spectrum (Average) are identical.

This is acquisition trace data and is shown for every enabled detector. It is not the Bluetooth Spectrum measurement result: the analyzed spectrum, with its Spec Limit line, is the Spectrum trace under the Bluetooth Spectrum group.

See Detectors and Power Spectrum Analysis for how each detector reduces the measured bins.

This trace is available only while the Average detector is enabled on the Detectors tab. Bluetooth Spectrum enables the detector selected by Detector automatically; any other detector must be enabled by hand.

See Also

Spectrum (Average)

Spectrum (Bluetooth Spectrum)

Available Trace Data