Error Summary (cdma2000/1xEV-DV)
When cdma2000/1xEV-DV demodulation is enabled, the trace data shows the composite error summary data. This is the signal quality error summary information for the composite signal.
For more information see the following topics:
There is also channel error summary trace data (), which provides the error information for a specific code channel and code layer (see Channel Error Summary Data)
See Also