Auto-select Highest SNR (Channel Sounding)

Auto-select Highest SNR automatically determines the reference channel with the highest SNR Signal-to-Noise Ratio in the peak of the impulse response. When Auto-select Highest SNR is cleared, the reference channel is determined by the Reference Measurement Channel parameter. Auto-select Highest SNR uses the results of the previous measurement.

When measurement averaging is enabled (Analysis > Average), make sure that you set the Reference Measurement Channel manually. When Auto-select Highest SNR is selected, the position of the impulse response will change if the reference measurement channel changes, which will affect the average.

Default: Enabled (selected)

See Also

Reference Measurement Channel

Format tab