Average Delay (sec) (Channel Sounding)
is a measure of the channel's average delay in seconds. This is the first moment of the power delay profile (PDP) trace. Basically, it is the “center of mass” of the PDP, and is expressed relative to the time of the first threshold crossing.
See Also