Path Include Mode (Channel Sounding)
specifies which impulse response points to include when computing RMS Delay Spread and Average Delay.
- Only points that are above the threshold (Threshold Reference + Threshold Offset) are included.
- Include all points between the first time the impulse response crosses the threshold (Threshold Reference + Threshold Offset) and the last time the impulse response crosses the threshold. This is the method used in ITU International Telecommunications Union: A United Nations agency that deals with telecommunications issues.-R P.1407-8.
Above Threshold
See Also