RMS Dly Spr Thresh (dBm) (Channel Sounding)
is the threshold used to determine whether a sample in the impulse response contains a path. This threshold is automatically set as 3 * sigma of the noise distribution (assumes AWGN Additive White Gaussian Noise - Statistically random radio noise characterized by a wide frequency range with regards to a signal in a communications channel.). You can adjust this threshold with the RMS Delay Spread Threshold parameter.
When averaging is enabled, is calculated from the averaged impulse response.
See Also
RMS Delay Spread Threshold