RMS Delay Spread (sec) (Channel Sounding)
is a measure of the channel's average delay spread in seconds, and is calculated from the content of the Sounding Ch Impulse Response trace using the following equations:
The paths are determined as those time samples whose power exceeds RMS Dly Spr Thresh.
When averaging is enabled, is calculated from the averaged impulse response.
See Also