About Component Test Measurement

The Component Test Measurement (8960120xC/U) feature provides a means to make repeatable channel response measurements such as group delay, phase linearity, and magnitude linearity.

Component Test measurement allows input channel configurations from one to four measurement channels. The Component Test results are computed independently for each measurement channel. For trace results, the measurement channel results are presented in an overlaid manner. For the summary table, measurement channels are presented in columns. For other measurement data (Time, Spectrum, Cross-Spectrum, CCDF Complementary Cumulative Distribution Function, etc.), traces are provided for each channel.

For more information, see Making a Component Test Measurement.

See Also

Selecting the Component Test Measurement feature

Making a Component Test Measurement