EVM (Component Test)

EVM is the RMS error-vector magnitude between the measured response and the reference, including linear channel-response effects. EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. is displayed in dB or percent according to the Show EVM in dB setting.

See Also

EVM (eq)

Available Summary Data