EVM (eq) (Component Test)
(Equalized RMS EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format.) is the residual error after the measured linear channel response is compensated. EVM (eq) is displayed in dB or percent according to the Show EVM in dB setting. EVM (eq) is only shown in Statistical Computation Mode.
See Also