IQ Gain Imbalance (Component Test)

IQ metrics are only available when Support Balanced/Unbalanced/IQ Responses is enabled.

IQ Gain Imbalance indicates the amount of amplifier gain imbalance between I and Q. For example, a value of -6.02 dB means the Q signal is being amplified twice as much as the I signal. This measurement is expressed in dB and calculated over the data in the Analysis Interval.

See Also

Available Summary Results      

IQ Offset

IQ Quad Err

IQ Time Skew