IQ Time Skew (Component Test)

IQ metrics are only available when Support Balanced/Unbalanced/IQ Responses enabled.

IQ Time Skew is the time difference between the I and Q parts of the signal. This value is calculated for the signal in the Analysis Interval.

One possible cause of IQ time skew is a difference in path length between the I and Q channels within the transmitter circuit.

See Also

Available Summary Results      

IQ Offset

IQ Quad Err

IQ Gain Imb