Copy Response to (Component Test)
copies the channel response for the selected path to Data Registers. When combined with the Fixed Equalization feature, this simplifies differential channel response measurements, or updating the measurement reference plane for the analyzer.
selects the Data Register(s) (Dx) for the channel response to be copied from the specified measurement channel(s). When combined with the Fixed Equalization feature, this simplifies relative channel response measurements, or updating the measurement reference plane for the analyzer.
See Also