Fixed Equalization (User Correction, Playback User Correction)

Acquisition > Playback User Correction

The Fixed Equalization properties apply a fixed FIR Finite Impulse Response equalization filter to the time data for the specified Measurent Channel. The filter is defined by its frequency response rather than by its impulse response. The frequency response must be stored in a data register. See About Fixed Equalization for more information.

When using segmented data (e.g. 5G NR Ch Freq Response), the first segment will be used and the others will be ignored.

Measurent Channel: When the measurement hardware or recorded signal has more than one input channel, choose the appropriate Measurent Channel. The equalization settings on the tab apply only for the Measurent Channel selected. (For more information, see Measurent Channel in Analog Input Properties).

Fixed Equalization: Select the Fixed Equalization check box to enable fixed equalization. Clear the check box to turn off fixed equalization.

See Also

About Fixed Equalization

Using Fixed Equalization

Using Fixed Equalization for Two-channel Measurements

Using Fixed and Adaptive Equalization Together